Alarm and Event Summary object model
Use the
FactoryTalk
Alarm and Event Summary object model to subscribe to, monitor, and interact with alarms and events from one or more areas in the FactoryTalk system. The Alarm and Event Summary:- Displays various alarm attributes.
- Indicates alarm states using icons and colors.
- Allows an operator to acknowledge, reset, suppress or disable the alarms that are displayed.
Provide Feedback