AlarmEventSummary object
The AlarmEventSummary object is the Alarm and Event Summary root object and represents an instance of an AlarmEventSummary. The AlarmEventSummary object is accessible from the container hosting an AlarmEventSummary object.
Provide Feedback