About the Alarm and Event Summary object model

Use the object model to programmatically control what an operator can see and do in the FactoryTalk Alarm and Event Summary object. The object model allows you to:
  • Control access to column values for the currently-selected row.
  • Modify the alarm filter.
  • Produce events when the user clicks or double-clicks a row.
  • Expose or conceal operations that affect the alarms and events system:
    • Acknowledging alarms.
    • Enabling or disabling alarms.
    • Removing events.
    • Filtering alarms and events.
    • Sorting alarms and events.
    • Printing alarms and events.
    • Finding alarms and events in the event list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal