EventItem object

The EventItem object represents a particular event selected in the Alarm and Event Summary and the Alarm and Event Banner. You can not create an EventItem object. It is accessible from the SelectedEvents property, EventClick event, and EventDblClick event of the AlarmEventSummary object.
The EventItem object is also accessible from the SelectedEvent property, EventClick event, and EventDblClick event of the AlarmEventBanner object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal