Action Group Properties

Use
Action Group Properties
to edit an action group or view the selected actions and action groups.
Setting
Description
Name
The name of the action group.
Action groups cannot be renamed once they are created. Instead, make a note of the permissions assigned to the action group and delete the action group. Add a new action group and give it the permissions noted.
Available actions and action groups
Shows the actions that are not already used in the action group. Select the actions to include in the new action group and then select
>>
to add them to the group.
Selected actions and action groups
Shows the actions in the new action group. To remove actions from the group, select the actions and then select
<<
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal