New Action Group
How do I open New Action Group?
- StartFactoryTalk Administration ConsoleorFactoryTalk View Studioand then log on to theFactoryTalkNetwork Directory orFactoryTalkLocal Directory.
- InExplorer, right-clickAction Groupsand then selectNew Action Group.
Group actions together to grant or deny security permissions for a set of actions in one step. Use
New Action Group
to add an action group. Specify the properties for each action group:Setting | Description |
---|---|
Name | Type a unique name for the new action group. The name cannot be the same as the name of any other action group. The name of the action group appears in Security Settings . The new action group appears in the category User Action Groups in the list of actions in the Security Settings .
|
Available actions and action groups | Shows the actions that are not already used in the action group. Select the actions to include in the new action group and select >> to add them to the group. |
Selected actions and action groups | Shows the actions in the new action group. To remove actions from the group, select the actions and select << . |
Provide Feedback