Add an action to an action group

To manage security settings for an action as part of an existing action group, add the action to the action group.
Prerequisites
Adding an action to an action group requires these permissions for the
Action Groups
folder in
FactoryTalk Administration Console
Explorer
:
  • Common > Read
  • Common > List Children
  • Common > Create Children
  • Common > Write
To add an action to an action group
  1. In
    FactoryTalk Administration Console
    Explorer
    , expand
    Action Groups
    , then right-click the action group to edit, and select
    Properties
    .
  2. In
    Properties
    , the action group appears on the right in the
    Selected actions and action groups
    list.
  3. In the
    Available Actions and Action Groups
    list, select the action to add to the action group, and select
    >>
    .
  4. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal