Action groups
Group the actions that can be performed on a resource. Define security once for the action group, rather than for each action separately.
When adding an action group decide:
- The name of the action group.
- What actions belong to that group.
Use action groups to assign permissions based on any convenient grouping. For example:
- A person's role or job (operator, supervisor, maintenance engineer, and so on).
- The equipment a person has access to (hoppers, mixers, ovens, and so on).
Once added, the action group the group appears in
Security Settings.
Right-click an item and select Security
. The new action group appears in the User Action Groups
category in the list of actions.Assign
Allow
or Deny
permissions to the action group, which then automatically assigns the permissions to the individual actions within the group.Beware of conflicting permissions
To help prevent conflicting permissions, cannot include (nest) action groups within other action groups.
The same action can be included in multiple action groups. This can cause conflicting permissions. For example, when the same action is included in two groups that apply to the same resource, and the first action group explicitly Allows permission, but the second action group explicitly Denys permission, the user is denied permission for the action that the two action groups have in common. Deny permissions always take precedence over Allow permissions.
Deleted action groups are not restored by creating a new action group using the same name
When an action group is deleted, any explicit permissions assigned to that group are no longer in effect.
For example, suppose an action group named "Operators" was used to explicitly grant write access to an area named "Mixing" for a user account "Chris". If the "Operators" action group is deleted, "Chris" can no longer write to the "Mixing" area. Creating another "Operators" action group will not restore "Chris" the ability to write to "Mixing".
If an action group is inadvertently deleted and restoring the FactoryTalk Directory from a backup is not feasible, all security permissions assigned to the resources that were using the action group must be recreated.
Provide Feedback