Select a FactoryTalk Directory to configure

The first step in configuring a
FactoryTalk Directory
is to select which
FactoryTalk
directory to configure from the first page in the
FactoryTalk Directory
Configuration Wizard
.
To select a
FactoryTalk Directory
to configure
  1. Go to
    Rockwell Software
    >
    FactoryTalk
    Tools
    >
    FactoryTalk Directory
    Configuration Wizard
    .
  2. In
    FactoryTalk Directory
    Configuration Wizard
    , under
    Configure settings
    , choose one or both of the following:
  3. Select
    Next
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal