Reset an expired password

When using the
FactoryTalk Directory
Configuration Wizard, if the password to the administrator account has expired,
Change Password
opens automatically. It cannot be opened manually.
TIP:
Alternatively, use
FactoryTalk Administration Console
or
FactoryTalk View Studio
instead of the
FactoryTalk Directory
Configuration Wizard to change an account password.
To reset an expired password
  1. In
    New password
    , enter the new password for the administrator account.
  2. In
    Confirm new password
    , enter the same password entered in
    New password
    , and select
    OK
    .
    Depending on how the
    FactoryTalk
    security policies are configured, minimum password length and password complexity requirements might apply.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal