FactoryTalk Directory Configuration Wizard

How do I run the
FactoryTalk Directory
Configuration Wizard?
  1. On the computer where
    FactoryTalk Services Platform
    is installed, log on to
    Windows
    with a user account that is a member of the local
    Windows
    Administrators group.
  2. Click
    Start > All Programs > Rockwell Software > FactoryTalk Tools > FactoryTalk Directory Configuration Wizard.
FactoryTalk Directory
products share a common address book, finding and providing access to plant floor resources, such as data tags and graphic displays.
Configuration of the
FactoryTalk Directory
is automatic during installation of
FactoryTalk Services Platform
. Use
FactoryTalk
Directory Configuration Wizard when circumstances require a manual configuration of
FactoryTalk Directory
. The
FactoryTalk Directory
Configuration Wizard is for use by
FactoryTalk
administrators.
Run the
FactoryTalk Directory
Configuration Wizard if:
  • An error occurs while installing the
    FactoryTalk Services Platform
    , or a message displays instructing to run the wizard manually.
  • A valid
    FactoryTalk
    Administrator account could not be found for the directory during an upgrade of an existing
    FactoryTalk Directory
    from
    FactoryTalk® Automation Platform
    version 2.0.
  • If
    FactoryTalk Services Platform
    was installed from a remote client (such as Remote Desktop Services). The
    FactoryTalk Directory
    cannot be configured from a remote client. The
    FactoryTalk Directory
    Configuration Wizard must be run at the
    Windows
    console on the computer.
  • The
    FactoryTalk
    administrator account in the network directory or local directory is not accessible. Running the wizard resets a locked administrator account, or changes an expired password for the administrator account. Alternatively, have another user whose account is a member of the
    FactoryTalk
    Administrators group reset your locked account or password for you.
If the administrator account was disabled, have another user enable the account in
FactoryTalk Administration Console
. The last
FactoryTalk
administrator account in a directory cannot be disabled. If no other user is available, or the password to another administrator account is not known (for example, because that user left the organization), contact
Rockwell Automation
Technical Support.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal