View a deleted user account
If the security policy
Show deleted accounts in user list
is enabled
, it is possible to view the properties of a deleted account. These properties cannot be modified.A deleted user account cannot be enabled; create a new account.
Prerequisites
Obtain these permissions in the
Users
folder in FactoryTalk Administration Console
Explorer
:- Common > List Children
- Common > Read
To view the properties of a deleted account
- Log into theFactoryTalk Directorythat contains the user account to delete.
- InFactoryTalk Administration ConsoleExplorer, expandSystem>Users, right-click the user account, and selectProperties.The user account properties are shown as they were when the account was deleted. Modifying the properties is not possible. The deleted account cannot be enabled.
- ClickCancelto close the properties sheet.TIP:An account can be deleted in one directory but remain active in the other.
Provide Feedback