User Properties

How do I open User Properties?
  1. Log on to the
    FactoryTalk
    network directory or local directory where you want to modify user accounts.
  2. In the
    Explorer
    window, expand the
    System
    folder until the user account you want to modify is visible.
  3. Right-click the user account you want to modify, and then click
    Properties
    .
To view and edit the settings for
FactoryTalk
user account
access, or the user's description in the system, use
User Properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal