Edit or view user account properties
Use these steps to view and edit the general properties of a
FactoryTalk
user
account, such as username and password, user description, user email address, and
user login method. These properties are only viewable for a Windows
-linked user account and cannot be edited. Use Windows
to edit the
general properties of a Windows
-linked user account.Prerequisites
Obtain these permissions in the
Users
folder in FactoryTalk Administration Console
Explorer
:- Common > List Children
- Common > Read
- Common > Write
To edit or view user account properties
- InFactoryTalk Administration ConsoleExplorer, expand theFactoryTalknetwork or local directory tree. Expand theSystem > Users and Groupsfolder to see the user account.
- Right-click the user account, and then selectProperties.
- Edit the following tabs:
- General
- Group Membership
- SelectOK.TIP:Changing the properties of aFactoryTalkuser account in oneFactoryTalkdirectory does not modify the properties in the other, even if the account has the same name in both directories. Before editing the properties of a user account, sign in to theFactoryTalkdirectory that contains the user account.
Provide Feedback