New Windows-linked User
How do I open New Windows-linked User?
In the
Explorer
window, expand System
> Users and Groups
, right-click Users
, point to New
, and then click Windows-linked User
.Use
New
to select Windows
-linked UserWindows
user accounts to link to the FactoryTalk
system. Windows
-linked user accounts are managed by Windows
. When accessing FactoryTalk
resources using a Windows
-linked account, FactoryTalk Directory
relies on Windows
to validate the user's name and password, and determine whether the account is enabled or locked out. Add user accounts to the
FactoryTalk
network or local directory from the list of users or groups in a Windows
domain or workgroup. If the computer is disconnected from the Windows
domain, the computer must reconnect to the domain before adding Windows
-linked user accounts. However, any users who previously logged on to the Windows
domain from that computer can log on to FactoryTalk
using their Windows
-linked user account while the computer is disconnected from the Windows
domain.If possible, use
Windows
-linked user group accounts rather than individual accounts. When deploying your applications from one domain to another, move the user accounts in a Windows
-linked user group from one domain to another by changing the domain the group belongs to. This allows moving the applications to a different domain without changing or recreating each user account separately, and without recreating all security permissions for the accounts.Windows-linked users are influenced by Windows security policy settings. For more
information, see The influence of Windows User Rights Assignment settings on a FactoryTalk system.
Provide Feedback