Server states
Server Status
displays the current state of the selected server. If the server is configured for redundancy, Server Status
also displays the state of the server's redundant partner. Server state | Description |
---|---|
<host> unreachable | This client computer cannot reach the computer hosting its server. This state applies if communications fail between this computer and the computer hosting the network directory server or HMI server. If the computer hosting a secondary server is disconnected from the network, communications between the primary server and the host server continue uninterrupted. The primary server remains active but displays a state of Active (Can't reach partner) . The secondary server displays a state of <host> unreachable . |
Active | The server is the active partner in an active-standby pair. If redundancy is not configured, the server is the Active server. |
Active (Can't reach partner) | A pair of servers is configured for redundancy, but one of the servers cannot connect with its partner. |
Failed | The server has failed. When redundancy is configured, the partner server provides service. |
Loading | The server's processes are starting up, and the server is currently loading processes and components. |
Not configured | Redundancy has not been configured for a secondary server. |
Not loaded | The server is not currently in use and has not notified the system that it is running. |
Ready to provide service | The server is ready to become the active server. |
Standby | The server is the Standby partner in an active-standby pair. This state does not apply if servers are not configured for redundancy. |
Starting | The server has finished loading its processes and components; it is currently reading configuration and performing other tasks in order to become available for use. |
Synchronized - ready to be Active | The server is ready to become the active partner in an active-standby pair. From this state, the server transitions immediately to the Active state. This state does not apply if servers are not configured for redundancy. |
Synchronized - ready to be Standby | The server is ready to become the standby partner in an active-standby pair. From this state, the server transitions immediately to the Standby state. This state does not apply if servers are not configured for redundancy. |
Synchronizing with Active | The server is transitioning into the Standby state. This state does not apply if servers are not configured for redundancy. |
Synchronizing with Standby | The server is transitioning into the Active state. This state does not apply if servers are not configured for redundancy. |
Provide Feedback