I do not see my imported resources

If you do not see imported resources listed in the
FactoryTalk Directory
when you open
FactoryTalk Administration Console
or
FactoryTalk View Studio
, you may need to:
  • refresh
    RSLinx Classic
  • use the
    Resource Editor
    instead of the
    Networks and Devices
    tree to edit security permissions for
    RSLogix 5000
    devices
To refresh
RSLinx Classic
  1. Go to
    Rockwell Software >
    RSLinx
    and run
    RSLinx Classic
    .
  2. To refresh
    RSLinx Classic
    , select
    RSWho
    .
    RSWho
  3. In the
    FactoryTalk Administration Console
    , right-click
    Networks and Devices
    , and then select
    Refresh
    .
To edit security permissions for a
RSLogix 5000
device
  1. In
    FactoryTalk Administration Console
    or
    FactoryTalk View Studio
    , in
    Explorer
    , right-click any application or area and then select
    Resource Editor
    .
    • If the
      FactoryTalk Directory
      does not contain any applications, at the top of the directory tree, right-click
      Network
      or
      Local
      and then select
      New Application
      . Type a name for the application, and then select
      OK
      . Right-click the application and then select
      Resource Editor
      .
  2. In
    Resources Editor
    , select the
    Add Resources
    button.
  3. In
    Select Resources for
    , expand the
    Logical Names
    folder.
  4. Right-click the name of the device and then select
    Security
    .
  5. Edit the security settings for the logical name of the device and then select
    OK
    .
    You do not have to add a logical name to an application or area for the security settings to take effect, unless you want the logical name to inherit its security settings from the application or area.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal