Explorer window

Shows the contents of the
FactoryTalk
Network Directory or
FactoryTalk
Local Directory in a tree view. To display the
Explorer
in
FactoryTalk Administration Console
or
FactoryTalk View Studio
, select
View > Explorer Window
.
To work with the options available for any item in the
Explorer
, expand the tree and right-click the item to open a context menu.
  • System folder
    — all of the items in the System folder apply to every application contained in the
    FactoryTalk Directory
  • Networks & Devices
    — displays the control hardware available to the local computer through
    RSLinx® Classic
  • Application tab
    — available only if
    FactoryTalk® Linx
    is installed.
  • Communications tab
    — available only if
    FactoryTalk Linx
    is installed. Displays the control hardware available to the local computer through
    FactoryTalk Linx
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal