Conversion instructions
Use Conversion instructions to convert the data type of a variable to a different data type.
Instruction | Description |
|---|---|
Converts a non-Boolean value to a Boolean. | |
Converts a value to a Byte. | |
Converts a String, Integer, Real, or Time data type to a Date data type. | |
Converts a value to a Double Integer. | |
Converts a value to a Double Word value. | |
Converts a value to an Integer. | |
Converts a value to a Long Integer. | |
Converts a value to a Long Real. | |
Converts a value to a Long Word. | |
Converts a value to a Real. | |
Converts a value to a Short Integer. | |
Converts a value to a String. | |
Converts a value to the Time data type. | |
Converts a value to an Unsigned Double Integer. | |
Converts a value to an Unsigned Integer. | |
Converts a value to an Unsigned Long Integer. | |
Converts a value to an Unsigned Short Integer. | |
Converts a value to a Word. |
Provide Feedback