ANY_TO_LREAL
The ANY_TO_LREAL instruction converts any value to a Long Real value.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the Micro810, L20E, L50E, and L70E controllers.
ANY_TO_LREAL

Parameter | Parameter Type | Data Type | Description | |
|---|---|---|---|---|
EN | Input | BOOL | When set to true, the instruction is enabled.
| |
i1 | Input | BOOL SINT USINT BYTE INT UINT WORD DINT UDINT | DWORD LINT ULINT LWORD REAL TIME DATE STRING | Any value other than a Long Real. |
o1 | Output | LREAL | A Long Real value. | |
ENO | Output | BOOL | Enables output. Applies to ladder diagram programs. | |
ANY_TO_LREAL structured text example
bres := ANY_TO_LREAL (true); | (* bres is 1.0 *) |
tres := ANY_TO_LREAL (t#1s46ms); | (* tres is 1046.0 *) |
ares := ANY_TO_LREAL (198); | (* ares is 198.0 *) |
Provide Feedback