ANY_TO_STRING
The ANY_TO_STRING instruction converts a value to a String value.
Operation details:
- When converting a REAL data type to a String, the ANY_TO_STRING instruction uses the IEEE 754 format.
- ANY_TO_STRING converts 125.0 to 1.25000E+02.
- When the target string length is 5 characters:
- ANY_TO_STRING converts 125.0 to 1.25000E+02 and outputs 1.250 to the target string.
- Consider creating a user-defined function block to convert from Exponential notation to number.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the Micro810, L20E, L50E, and L70E controllers.
ANY_TO_STRING

Parameter | Parameter Type | Data Type | Description | |
|---|---|---|---|---|
EN | Input | BOOL | When set to true, the instruction is enabled.
| |
i1 | Input | BOOL SINT USINT BYTE INT UINT WORD DINT UDINT | DWORD LINT ULINT LWORD REAL LREAL TIME DATE | Any value other than String. |
o1 | Output | STRING | If IN is a Boolean, 'FALSE' or 'TRUE'. If IN is an Integer or a Real, a decimal representation. If IN is a TIME, can be:
| |
ENO | Output | BOOL | Enables output. Applies to ladder diagram programs. | |
ANY_TO_STRING structured text example
bres := ANY_TO_STRING (TRUE); | (* bres is 'TRUE' *) |
ares := ANY_TO_STRING (125); | (* ares is '125' *) |
Provide Feedback