ANY_TO_BYTE
The ANY_TO_BYTE instruction converts a value to an 8-bit Byte value.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the Micro810, L20E, L50E, and L70E controllers.
ANY_TO_BYTE

Parameter | Parameter Type | Data Type | Description | |
|---|---|---|---|---|
EN | Input | BOOL | When set to true, the instruction is enabled.
| |
i1 | Input | BOOL SINT USINT INT UINT WORD DINT UDINT DWORD | LINT ULINT LWORD REAL LREAL TIME DATE STRING | Any non-Byte value. |
o1 | Output | BYTE | An 8-bit Byte value. | |
ENO | Output | BOOL | Enables output. Applies to ladder diagram programs. | |
ANY_TO_BYTE structured text example
bres := ANY_TO_BYTE (true); | (* bres is 1 *) |
tres := ANY_TO_BYTE (t#0s46ms); | (* tres is 46 *) |
mres := ANY_TO_BYTE ('0198'); | (* mres is 198 *) |
Provide Feedback