Create a String Input Enable button
At runtime, the operator can use the
String Input Enable
button to open a string pop-up keyboard or scratchpad. When the operator presses the button, the pop-up opens. The operator can use the pop-up to enter a string value to send to the Value connection at the data source.To create a String Input Enable button
- In theGraphics Displayeditor, selectObjects > Numeric and String > String Input Enableor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks, the button’s tags, whether to use the string pop-up keyboard or scratchpad, and whether to use Enter key handshaking.
Provide Feedback