Options on the Timing tab of the String Input Enable Properties dialog box
The following table shows the options on the
Timing
tab of the String Input Enable Properties
dialog box.Options | Descriptions |
|---|---|
Timing and handshaking settings | |
Enter key control delay | Select the time to delay between the time the operator presses the Enter button and the time the application sets the Enter connection to 1. |
Enter key hold time | Select the time the Enter connection will be set to 1. This time setting applies only if the Enter connection is assigned and the Enter Handshake connection is not assigned. |
Enter key handshake time | Select the maximum time the Enter connection will be set to 1. This time setting applies only if the Enter and Enter Handshake connections are both assigned. |
Handshake reset type | Select how the Enter Handshake connection resets the Enter connection to 0:
|
Provide Feedback