Keys on the external keyboard or keypad
The external keyboard or keypad has the following keys:
- Insert/OverstrikePress theInsertkey to toggle between insert and overstrike modes.
- Left arrowPress theLeftarrow key to move the cursor to the left.
- Right arrowPress theRightarrow key to move the cursor to the right.
- EscapePress theEsckey to close the pop-up without writing the string to the Value connection.
- DeletePress theDeletekey to clear the scratchpad.
- BackspacePress
to delete the character to the left of the cursor. Hold the button down to delete multiple characters. - EnterPress
to write the string to the Value connection.
Provide Feedback