Keys on the external keyboard or keypad
The external keyboard or keypad has the following keys:
- SEL [F1]PressF1on the keyboard to write the selected character to the scratchpad.
- Insert/Overstrike [F2]Press the F2 key to toggle between insert and overstrike modes.
- << [F3]PressF3to move the cursor in the scratchpad to the left.
- >> [F4]PressF4to move the cursor in the scratchpad to the right.
- CLR [F5]PressF5or theDeletekey to clear the scratchpad.
- BackspacePress the
to delete the character to the left of the cursor. Hold the button down to delete multiple characters. - Left arrowPress theLeft arrowkey to move the character highlight to the left.
- Right arrowPress theRight arrowkey to move the character highlight to the right.
- Up arrowPress theUp arrowkey to move the character highlight up to the next higher row.
- Down arrowPress theDown arrowkey to move the character highlight down to the next row down.
- EscapePress theEsckey to close the pop-up without writing the string to the Value connection or text box.
- EnterPress theEnterkey to write the string to the Value connection of a string input enable button or to the text field in theLogin or Change Passworddialog box.
Provide Feedback