Settings and controls
You can use the main page to view and manage machines and activations and perform
administrative tasks. Use the icons in the taskbar at the top of the page to perform
tasks.
Select the view icons on the left side of the page to view machines and activations.
Icon | Description |
|---|---|
Find Machines | Opens the Find Machines dialog box. Use the dialog box to find
and group machines. |
Scan | Performs a scan and refreshes the machines and activations information. |
Export | Exports a list of machines, activations, Add-On Profiles (AOPs), or the log to a
.csv file. |
Switch Server | Selects the server to view or adds a server to the list. |
Schedule | Sets the schedule for automatic scanning of all machines. Enter the interval, in
days, at which scans should occur. |
Account | Opens the Account dialog box, to sign in to the Rockwell
Automation Product Compatibility and Download Center (PCDC) and the FactoryTalk
Updater Server. You can also switch users on the server. See Switch user accounts on a server. |
Download Location | Specifies the location for downloaded files. |
Preferences | Select to view details for the installed version of FactoryTalk Updater. |
Provide Feedback