Machines view
In the View menu, select
to display a list of all machines or a list of machines in a group. Enter a term in the
Machines
Search
box to highlight that term in the list.Column | Description |
|---|---|
Name | The name of the machine. Select Expand
Tip: Name displays only the first 15 characters in the machine
name. Names longer than 15 characters are truncated. |
Address | The IP address of the machine. |
Status | The online or offline status of the machine. |
Installed Version | The installed version of software. The Version Lifecycle Management (VLM) icon
indicates the lifecycle status for the installed version:
|
Latest Version | The newest version of software available on the Rockwell Automation Product
Compatibility and Download Center. |
Latest Patch | The newest software patch available on the Rockwell Automation Product
Compatibility and Download Center. |
Activations | The activation search path. |
FactoryTalk Updater R4.10 allows you to verify the operating system version of the agent both
client and web client, that the installed FactoryTalk Updater Agent version is greater than or
equal to v4.10, and that FactoryTalk Updater Agent can collect the operating system
information and send it to FactoryTalk Updater Server.
Verify the operating system version of the machine by mousing over
on the client.
Provide Feedback