TRANSACTIONS tab
The TRANSACTIONS tab in the Activations view displays a log of license events, or
transactions, for all machines or machines in a group. To prevent transaction log files from
growing too large, FactoryTalk Updater saves transactions for four months and then discards
them.
Column | Description |
|---|---|
Time | The date and time the transaction occurred. |
Activity | The type of transaction; for example, a license return, borrow, check out, rehost,
or get. |
Machine Name | The name of the machine that carried out the transaction. |
Username | The user who conducted the transaction. |
Feature Name | The executable file for the licensed Rockwell Automation software application; for
example, RS5000.exe. |
Product | The name of the licensed Rockwell Automation software application. |
Serial Number | The serial number of the licensed Rockwell Automation software application. |
Quantity | The number of licenses included in the transaction. |
Provide Feedback