License Information tab
The
LICENSE INFORMATION
tab in the Activations view lists license information
for all machines or for machines in a group. Enter a search term in the Search box to
highlight that term in the list. Column | Description |
|---|---|
Product | The Rockwell Automation software application. |
Serial # | The serial number of the product. |
Expires | The expiration time and date for the activation. |
Activation | The name of the activation. |
Feature Version | The feature version of the license. |
Location | The machine name of the activation server. Tip: The Location box displays only the first 15 characters in
the activation server name. Names longer than 15 characters are truncated. |
Total | The number of activations purchased with the product. |
In Use | The number of activations used for each product. Select the number in this column
to see more details, such as the computer that checked out or borrowed the
activation, the number of activations checked out or borrowed, and whether the
activation is concurrent or borrowed. No details are available if the number in this
column is zero. |
Borrowed | The number of activations borrowed from an activation server. Select the number in
this column to see more details, such as the computer that borrowed the activation,
the date the activation was borrowed, and the date the borrowed activation expires.
No details are available if the number in this column is zero. |
Product Version | The product version activated. Some activations are for multiple product versions.
This field displays n/a if not used. |
Provide Feedback