Protection view
The motor protection system monitors and measures AC motor current to ensure that the motor operates within its limits and remains protected in case of mechanical system issues that could result in failures.
Section | Description |
|---|---|
Trip class | Displays the read only value of "Trip class" selected in the "Overload" sub view. |
FLA | Displays the read only value of "FLA" selected in the "Overload" sub view. |
Warning limit | Displays the read only value of "Warning limit" selected in the "Overload" sub view. |
Auto reset overload trip | Displays the read only value of "Auto reset overload trip" selected in the "Overload" sub view. |
Data communication fault trip | Displays the read only value of "Data communication fault trip" selected in the "Overload" sub view. |
Show only enabled trips and warnings | This checkbox sorts the Table column. When selected, the columns are hidden or visible based on the user configuration for a specific trip or warning. When unselected, both the Jam and Underload columns are visible. |
Section | Description |
|---|---|
Inhibit mode | Displays the read only value of "Inhibit mode" selected in the "Jam" or "Underload" sub view respectively. |
Inhibit time | Displays the read only value of "Inhibit time" selected in the "Jam" or "Underload" sub view respectively. Both values are in seconds. |
Trip delay | Displays the read only value of "Trip delay" selected in the "Jam" or "Underload" sub view respectively. Both values are in seconds (s). |
Trip limit | Displays the read only value of "Trip limit" selected in the "Jam" or "Underload" sub view respectively. Unit is % FLA. |
Warning delay | Displays the read only value of "Warning delay" selected in the "Jam" or "Underload" sub view respectively. Unit is seconds (s). |
Warning limit | Displays the read only value of "Warning limit" selected in the "Jam" or "Underload" sub view respectively. Unit is %FLA. |
Provide Feedback