Jam view
The Jam view enables the trip and warning if a jam condition occurs. If the motor current has exceeded a set level, this indicates that a mechanical jam has occurred. Fast response time is vital to reduce the potential for damage to the mechanical system and motor.
Item | Description |
|---|---|
Enable trip / warning on jam | Enables/disables the trip and warning if jam conditions occur. Other configurations of the jam settings are dependent on this checkbox. If enabled, all other fields on the "Jam" view are not editable and display the grayed out values present in the respective config structure member. |
Section | Description |
|---|---|
Inhibit mode | Set the jam inhibit mode. |
Inhibit time | Set the jam inhibit time in seconds. |
Section | Description |
|---|---|
Trip limit | Set the jam trip level in %FLA. |
Trip delay | Set the jam trip delay time in seconds. |
Section | Description |
|---|---|
Warning limit | Set the jam warning level in %FLA. |
Warning delay | Set the jam warning delay in seconds. |
Provide Feedback