Underload view
The Underload view enables or disables the trip and warning if an underload condition occurs. The system has experienced an undercurrent, which may indicate a mechanical change. Detecting this fault rapidly can help minimize damage and reduce production downtime.
Item | Description |
|---|---|
Enable trip or warning on underload | If checked, enables/disables the trip and warning if an underload condition occurs. Other configurations of the underload settings are dependent on this checkbox. If unchecked, all other fields on the "Underload" view are not editable and displays the grayed out values present in the respective config structure member. |
Section | Description |
|---|---|
Inhibit mode | Sets the configuration of the underload inhibit mode. |
Inhibit time | Sets the configuration of the underload inhibit time in seconds. |
Section | Description |
|---|---|
Trip limit | Set the underload trip level in %FLA. |
Trip delay | Set the underload trip delay time in seconds. |
Section | Description |
|---|---|
Warning limit | Set the underload warning level in %FLA. |
Warning delay | Set the underload warning delay in seconds. |
Provide Feedback