Overload
The Overload appears when the motor surpasses its thermal rating due to an overload. An overload occurs when the motor draws excessive current over a specific period, resulting in increased heat within the motor. Over time, this can lead to significant damage to both the motor and surrounding systems.
Section | Description |
|---|---|
Trip class | Sets trip class, which is a time taken by the relay to open in case of overload condition. |
FLA | Sets the full load current settings for Overload in unit Amps. Value allows one digit after a decimal point. |
Warning limit | Sets the Overload warning limit in %TCU. |
Trip reset mode | Sets the reset mode in case of any overload trip action. |
Provide Feedback