Module Tag Definitions
The tags that are available vary depending on module type and selections made in the
Device Definition.
The types of module tags include:
- Configuration (as indicated by "C")
- Input (as indicated by "I")
- Output (as indicated by "O")
- Event Input (as indicated by "EI")
- Event Output (as indicated by "EO")
Provide Feedback