Add FTAE content

Add
FactoryTalk Alarms and Events
content to library objects to support Logix digital alarm applications. There is separate content for the digital alarm definition, the alarm message, and the alarm tag update rate.
IMPORTANT:
Refer to the
FactoryTalk Alarms and Events
System Configuration Guide
(
Rockwell Automation
Publication FTAE-RM001) for more information on the screens and settings associated with
FactoryTalk Alarms and Events
content.
To add
FactoryTalk Alarms and Events
content to a library object
  • Right-click the library object in the
    Library Content
    column and select
    Add Section > FTAE
    . An
    FTAE
    folder, with subfolders for
    Digital Alarms
    ,
    Messages
    , and
    Tag Update Rates
    , is added to the library object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal