Delete message content
If a message is no longer needed, it can be deleted from
Library Object Manager
.To delete a message from a library object
- InLibrary Repositories, select a library object that includes Logix tags.
- InLibrary Content, expand theFTAEfolder and then click theMessagesfolder.
- ThePropertiespanel displays a listing of all existing messages when theMessagessubfolder is selected.
- Right-click the message listing and then clickDelete.If the message is used in a digital alarm, a confirmation dialog appears listing the alarms that use the message. ClickYesto continue with the deletion. The alarms using the message no longer have an alarm message.
Provide Feedback