Message Editor dialog box

Alarm messages describe alarm conditions. Use the
Message Editor
to create the messages needed for different alarms. Each alarm can be associated with only one message.
This table describes the settings in the
Message Editor
.
Name
Setting Type
Description
Message
Text entry
The message appears here as it is compiled. Text can be entered directly in this setting. Variable tags are added when
Add
is clicked.
Add Variable
Variable
Dropdown menu
A list of tags that can be added to the message. This includes a number of default variables, as well as up to four variables added defined by
Associated Tags
settings in the
Properties
panel.
Data Type
Dropdown menu
Where applicable based on the Tag selected, offers a choice of numeric or string for the data type of the Tag value within the message.
These settings appear if
String
is selected in the
Data Type
setting.
Use Fixed Width
Checkbox
Limits the amount of information displayed for the tag value within the message to the value entered in the
Number of Characters
setting.
Number of Characters
Text entry
Sets the maximum number of characters to display for the tag value within the message.
These settings appear if
Numeric
is selected in the
Data Type
setting.
Number of Digits
Text entry
Sets the number of digits to display for the tag value within the message.
Decimal Places
Text entry
Sets the number of decimal places to display for the tag value within the message.
Left Fill
Dropdown menu
Determines whether values will be filled in to match the value set for
Number of Digits
. Values used to fill in the space can be either zeros or spaces.
Add
Button
Adds the currently selected tag to the message.
ID
Text entry
The unique numeric ID for the message.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal