Add an existing message
Alarm messages can be created independently from alarms and then added to the alarm.
To add an existing message to a digital alarm
- InLibrary Repositories, select a library object that includes Logix tags.
- InLibrary Content, expand theFTAEfolder and theDigital Alarmsfolder.
- In theDigital Alarmsfolder, select the alarm object, thePropertiespane displays the digital alarm properties.
- UnderMessage, click theBrowsebutton. TheMessage Browseropens.
- TheMessage Browserdisplays all messages within the current ACD file. Select a message and clickOK.IMPORTANT:The value within the ID setting for each message must be unique for all digital alarm messages within a project. Messages added using theMessage Browserretain their original ID.
Provide Feedback