Create an image
Use the image tool to place bitmap, JPEG, PNG, or SVG images on a display. For monochrome images, you can set up the image to blink at runtime.
- For monochrome images, the background color becomes transparent when you change the Image back style to Transparent.
- For color images, any area of the image that is black becomes transparent when you change the Image back style to Transparent.
Before you can place an image on a display, you must import the image into the application.
To place an image in a display:
- In theGraphicseditor, selectObjects>Drawing>Image,or click the image icon in the toolbox.
- Drag the mouse to position and draw a rectangle the general size and location you intend the display to be.
- Double-click the object to open theImage Propertiesdialog box.
- In the property tabs, specify the image to use and how you intend the image to look.
Provide Feedback