Image Properties - General tab
The following table shows the options in the
General
tab of Image
Properties
.Options | Description |
|---|---|
Image | Select the file name of the graphic image for the object or state. The image appears on the face of the object, to give the operator information about what the object does or about the current state. Before you can place an image on the object, you must import the image into the application. |
Image back style | Click the down arrow and then click Solid or Transparent to specify the object’s background style. For color images except for PNG with Alpha channel and SVG, if the Image back style is set to Transparent, any parts of the image that are black will be transparent. |
Image color | For monochrome images, this field displays the current image foreground color. Click it to select another color. |
Image back color | For monochrome images, this field displays the current image background color. Click it to select another color. If the image background style is transparent, the application does not use this image background color. |
Image blink | For monochrome images, select this check box if the image is to blink at runtime. The image blinks twice per second. |
Provide Feedback