Set up how the image looks

Use the
Image Properties
to set up how the image looks.
To set up general options for the image:
  1. In a display, double-click the object to open the
    Image Properties
    dialog box.
  2. Specify the image to use and its appearance.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal