Create a radar chart object

A radar chart is a graph used as a multi-parameter data comparison tool. It is created using the radar series, which renders the data as a series of lines radiating out from the center. Use the radar chart to compare multiple data points and identify the variation across different categories.
To create a radar chart object
  1. In FactoryTalk View Studio, in the Graphic editor, open a display.
  2. On the toolbox, select
    Advanced
    >
    Radar Chart
    .
  3. On the display, drag the mouse to draw the approximate size that the radar chart object is to be.
  4. In the
    Radar Chart Properties
    dialog box, on the
    General
    tab, select
    Radar Chart Setup
    .
    1. On the
      Common
      tab, configure radar categories, series, and their associated tags.
    2. On the
      Appearance
      tab, configure chart background, radar shape, radar appearance, decimal place for data points, and refresh rate.
  5. Select
    Preview
    to see the configured radar chart.
  6. (optional) Select
    Set as default
    to save the current configuration as default for objects to be created.
  7. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal