Radar Chart - Appearance tab

Use this tab to configure chart background, radar shape, radar appearance, decimal place for data points, and refresh rate. The following shows the options on the tab.
TIP:
Select
Preview
on the right side of the dialog box to see the configured radar chart.
Select
Set as default
to keep the current configuration for radar charts to be created.
Option
Description
Font setting
Configure the style and color for categories, legend, and data labels.
Radar shape
Specify the shape of the chart.
Chart background
Specify the color of the chart.
Grid line
Specify the look and color of the grid line.
Banded color
Specify the banded color of the chart.
Show legend
Specify whether to show the legend and its position on the chart.
TIP:
Make sure the object size is big enough to show the entire legend.
Decimal place
Specify the decimal place of data on the chart.
Refresh rate
Specify how often in seconds the chart refreshes its data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal