Radar Chart - Common tab
Use this tab to configure radar categories, series, their associated tags, and line appearance. The following shows the options on the tab.
TIP:
Select
Preview
on the right side of the dialog box to see the configured radar chart.Select
Set as default
to keep the current configuration for radar charts to be created.Option | Description |
|---|---|
Chart title | Configure the chart title, font, size, style, and color. |
Series count | Specify the number of series on the radar chart. A series is a group of data points for you to compare.
The supported maximum series count is six. |
Categories count | Specify the number of categories on the radar chart. Each category represents an axis. Series are compared across the defined categories.
The supported maximum categories count is 50. |
Common | |
Category | Specify the name of each category. |
Min Value | Specify a category's minimum value, which is the center point of the radar chart. |
Max Value | Specify a category's maximum value, which is the end point of the radar chart. If the value is greater than the maximum value, the series line will show outside of the chart. |
Tag | This column is read-only on the Common tab. Configure tags on the Series tab. |
Series | |
Category , Min Value , and Max Value | These columns are read-only on the Series tab. Configure them on the Common tab. |
Tag | Specify a tag or a constant value for each category. You can click the browse button to open the Tag Browser to browse tags. |
Series name | Specify series names that will show as legend on the chart. To show or hide the legend, configure it on the Appearance tab. |
Line and marker | Specify the look for series lines and markers on the chart. |
Line color | Specify the color for series lines and their markers. |
Fill color | Specify the color for the fill area. |
Provide Feedback