Data source configuration
Configure data sources to populate a namespace and collect data from data tags and
FactoryTalk Smart Object
instances. Data tags are accessed from controllers, devices, and servers. FactoryTalk Smart Object
instances require an offline Studio 5000 Logix Designer
project file (.acd) to populate the namespace and an EtherNet/IP driver for data collection.FactoryTalk Edge Gateway
gathers the directory of data from the source and stores the data into a namespace. In the case of FactoryTalk Smart Object
instances, the FactoryTalk Smart Object
model is also discovered and replicated in Models
. Use these data tags and models to configure the gateway.From
Configure Data Sources
, add, edit, delete, populate, clear, and filter data sources.Data Source Types
Add tags and
FactoryTalk Smart Object
instances for these data source types:- Studio 5000 Logix Designerproject file
- Logix Controller via EtherNet/IP
- FactoryTalk Live Datashortcut
- Drive/IMC device
- OPC DA device (standalone version only)
- KEPServer Enterprisedevice (standalone version only)
Namespace
A namespace is a directory of data from your data sources or a collection of data types and instances. The namespace is a local representation of the data structure from the source. The namespace enables quick sorting and searching across all data sources when building models and configuring data to applications. Most namespaces support online discovery of data from data sources. For
FactoryTalk Smart Object
instances or offline configurations, use .acd files to generate a namespace and create models before deploying the data to applications.Collection path
Define the collection path when configuring data sources. The collection path defines the location where
FactoryTalk Edge Gateway
gathers data. This collection path and namespace often use the same path. When configuring an offline Logix Project File data source type, define a collection path to enable FactoryTalk Edge Gateway
to collect the system data for running applications.An icon shows the status of the
Driver
and Collection Path
for each configured data source:Icon | Description |
|---|---|
![]() | The driver is offline. The collection path is inactive. |
![]() | The driver is paused. |
![]() | The driver is running. The collection path is active. |
Provide Feedback