Add a data source from a FactoryTalk Live Data Shortcut
Add data sources from
FactoryTalk Live Data
to populate a namespace and collect data from data tags. The data source is also a shortcut to these source types: HMI TagDb, OPC DA server, OPC UA server, and FactoryTalk® Linx™
shortcut.The
FactoryTalk Live Data Shortcut
data source is compatible with the FactoryTalk Live Data
driver.To add a data source from a
FactoryTalk Live Data
shortcut- SelectData Flow>Data Sources, and fromConfigure Data Sources,add a data source.
- To add the first data source, selectAdd Data Sources.
- To add a subsequent data source, selectAdd
.
- Enter the nameand then fromData Browse Path Type,selectFactoryTalk Live Data Shortcut.
- The name must contain only letters, numbers, and hyphens.
- FromDriver for browsing,select theFactoryTalk Live Datadriver.
- Select a network or local path and enter the browse path.
- (optional) To automatically generate the namespace, selectAuto-populate namespace.
- Perform one of these:
- SelectUse browse path for data collection.
- FromDriver for Collection, select theFactoryTalk Live Datadriver for the data collection path and enter the collection path.
- SelectSaveto add the data source.
Provide Feedback