Populate data sources
Populating a data source gathers data from a controller, device, or server and saves the data in the namespace. The namespace tracks tags and
FactoryTalk Smart Object
from the data source.After adding new tags to data sources previously configured in
FactoryTalk Edge Gateway
, repopulate the data sources to synchronize the new tags with the namespace.
TIP:
To generate the namespace, select
Auto-populate namespace
when configuring a data source.To populate a data source
- SelectData Flow>Data Sources.
- (optional) FromConfigure Data Sources, filter the list of data sources.
- Select the data sources to populate.
- SelectPopulate
to update the namespace for the data sources. TheStatusof the data sources displaysPopulated.
Provide Feedback