Add a data source from a Drive/IMC Device
Add data sources from drives or Integrated Motion Control (IMC) devices to populate a namespace and collect data from data tags.
The
Drive/IMC Device
data source is compatible with the EtherNet/IP (CIP)
driver.To add a data source from a Drive/IMC Device
- SelectData Flow>Data Sources, and then fromConfigure Data Sources,add a data source.
- To add the first data source, selectAdd Data Sources.
- To add a subsequent data source, selectAdd
.
- Enter the nameand then fromTags and types defined in (data browse path type), selectDrive/IMC Device.
- The name must contain only letters, numbers, and hyphens.
- FromDriver for browsing,selectEtherNet/IP (CIP) driver.
- Enter the browse path.
- (optional) To generate the namespace, selectAuto-populate namespace.
- Perform one of these actions:
- SelectUse browse path for data collection.
- FromDriver for Collection, select the EtherNet/IP (CIP) driver for the data collection path and then enter the collection path.
- (optional) To populate only symbolic tags into the namespace, selectPopulate only Symbolic Tags (Smart devices).
- SelectSaveto add the data source.
Provide Feedback