Understand eProcedure security
e
ProcedureThere are distinct differences between the security capabilities of the Client and the
FactoryTalk
e
ProcedureFactoryTalk Batch
View:- Command buttons in theClient are shown, but disabled, if the user does not have the appropriate permissions.eProcedure
- TheReactivatebutton on the Instructions view of theClient and the StepeProcedureReactivateStepConfirm policy setting inFactoryTalkDirectory are specific to.eProcedureTIP: Because the ability to secureFactoryTalkinstruction files does not currently exist ineProcedureFactoryTalkSecurity, you can require an electronic signature on Parameter Change to prevent unauthorized users from executing instructions. (SeeElectronic signaturesin the for more information.)
Provide Feedback